Feedback_Kp

Feedback_Kp

Address: 10240 (2800H)
Type: Unsigned32
Access: Read/Write
Unit: --
Range: Unsigned32
Default Value: 20000
Store Supported: Yes
Description:

This value is used for Feedback feature and define the position Gain of PID’s regulator. The value has to be adjust to keep the Feedback_Actual_Position_Error inside the tolerance of application. The value can be set to 0, when is necessary only a velocity controller and has not to be considered the position error.

Pay attention that a not coherent value (big value) can introduce motor’s vibration.

Notes: See Closed Loop Modality for details.